Part Number: MSPM0G1507
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
Our customer is having a problem with bricking their boards in production. It isn’t 100%.
They have had no issues with the XDS110. They have had no problems with their US based CGANG.
However overseas at their CM, they are seeing ~50% fallout.
The CM is using a CGANG developed by Elprotronic.
These board do run – and they can see the boards exhibiting correct behavior HOWEVER – they cannot communicate with them.
They have tried the web based tool and Uniflash to restore the stocks to a communicative state - but no luck.
They have written a custom boot loader that is UART based. However – it is not doing the reprogramming – that is being done by the CGANG over SWD.
I have done some easy troubleshooting looking at getting the ROM BSL turned off in Sysconfig.
My gut tells me we are currupting non-main with the Elprotronic setup. I'll send you screenshots of the configuration offline.
Ideas?
Thanks!
Blake