Other Parts Discussed in Thread: HALCOGEN
Hello,
I'm using in my application the module DCC1, where Clock Source 0 is HF_LPO and Clock Source 1 is PLL1. I made the complete configuration in HalCoGen and then generated code. Additionally, I mapped the DCC1 error signal to the Error Signaling Module's group1 channel 30.
I can easily provoke the DCC1 error signal when I change the Count 0 or Count 1 to an invalid value. However, I receive the DCC1 error signal even if the Count 0 and Count 1 are correct and all other settings seem to be fine as well. In this case, the DCC1 error signal arises sporadically, it takes a few seconds or sometimes even a few minutes. In fact, when I touch the oscillator on my eval board (RM48 HDK), then it arises almost immediately. It seems that the oscillator provided on the eval board is rather sensitive to external disturbances, or the HF_LPO is not providing the correct signal. What else can the matter be? Did you observe the same effect?
Thank you
Regards
Vaclav