Part Number: SYSCONFIG

II am trying to configure a LED for WAKEUP R5 in AM62A-Q1 but i am not able to open the GPIO window itself.
Is there something I am missing.
Regards
Aakash T
I can see the same issue.
If I import an example by default it uses SysConfig 1.24. I can add GPIO fine.
I close SysConfig.
Change the project to use 1.28
Open SysConfig again.
Try to add GPIO and I see the error.
I can confirm this is a bug on the SDK/Device data side after doing some testing. We will follow up with the device and SDK teams.
For now we would recommend using SysConfig 1.27 or earlier with this SDK.
Hello Akash, SDTO team,
I've re-assign this thread to the correct engineer. Please allow some time for a response.