Part Number: MSPM0L1306
Other Parts Discussed in Thread: MSPM0G3507
For the MSPM0L1306,
Framing-error detection is required for LIN conformance, including framing errors in the sync, PID, data, and checksum fields.
But the TRM states: "Framing errors and break conditions are not set when LIN mode is enabled."
For LIN break-threshold detection, it must be operated in LIN Mode, utilizing LINCNT, LINC0, and the following LINCTL settings, which stops the framing-error detection as the side-effect.
Newer MSPM0L devices (MSPM0L211x/122x) come with UNICOMM-UART which has an additional setting LINCTL.EN_FRM_ERR, allowing framing-error reporting during LIN operation:
But the MSPM0L1306 UART does not provide this field:
So,
How can framing-errors be detected on the MSPM0L1306 while using the LIN counter for break-threshold detection?
If simultaneous operation is not supported, what is TI’s recommended implementation for meeting both requirements?
1. Break detection with an 11-Tbit threshold
2. Framing-error detection for LIN Conformance Tests
Thanks in advance,
Zaigham