Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2612: AM261x issues configuring custom CiA402 PDOs using Beckhoff SSC Tool

Part Number: AM2612

Hi Experts,

I am working on a custom board featuring the AM2612 SoC and aiming to implement EtherCAT CiA 402 with custom PDO definitions. I am using the INDUSTRIAL-COMMUNICATIONS-SDK-AM261X (version 2026_00_00_06) and referring to the Official Documentation (EtherCAT SubDevice Beckhoff SSC Demo).

I have encountered two issues when using the Beckhoff SSC Tool (v1.5.3.0) to configure PDOs and generate the source code:

1. Missing TI_ESC_CiA402_8i3.xml in SDK release According to the SDK documentation and the README.txt under ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/beckhoff_stack/patch/am261x/, there should be two XML files:

  • TI_ESC_8i3.xml

  • TI_ESC_CiA402_8i3.xml

image.png

image.png

However, checking the actual directory in SDK v2026.00.00.06 reveals that TI_ESC_CiA402_8i3.xml is missing (only TI_ESC_8i3.xml, tiescappl.xlsx, and README.txt exist).

image.png
Additionally, in the parent directory ${SDK_INSTALL_PATH}/source/industrial_comms/ethercat_subdevice/beckhoff_stack/patch/, there is a TI_ECAT.patch file. Is there a separate patch file required specifically for CiA 402 implementation?

2. Importing custom PDO Excel overrides CiA402_SAMPLE_APPLICATION back to 0 To work around the missing XML file, I modified TI_ESC_8i3.xml as follows:

  • Set CiA402_SAMPLE_APPLICATION from 0 to 1

  • Changed APPLICATION_FILE from tiescappl.h to cia402appl.h

  • Removed <ApplicationFile>tiescappl.xlsx</ApplicationFile>

When importing this modified XML into a new SSC project, CiA402_SAMPLE_APPLICATION is correctly set to 1 and APPLICATION_FILE is set to "cia402appl.h". However, after importing a custom Excel file containing custom PDO configurations (where Device Profile is set to 402 and objects conform to CiA 402 specifications), SSC Tool automatically:

  • Resets CiA402_SAMPLE_APPLICATION back from 1 to 0.

  • Changes APPLICATION_FILE to <project_name>.h.


Below is the step-by-step workflow of how I configured the project using the Beckhoff SSC Tool:

1. Step 1: Created a new project using my modified TI_ESC_8i3.xml configuration file.

new_project.png
2. Step 2 : Prior to importing the custom PDO Excel file, CiA402_SAMPLE_APPLICATION is set to 1, and APPLICATION_FILE is set to #include "cia402appl.h".

before_import_xlsx.png
3. Step 3: Saved the project configuration under the name "test".

save_project_name_as_test.png
4. Step 4: Selected the custom PDO Excel configuration file (test.xlsx).

import_xlsx.png
5. Step 5: Imported the custom PDO Excel configuration file.

import_xlsx2.png
6. Step 6: After the import completed, checking the Application node in SSC Tool shows that CiA402_SAMPLE_APPLICATION was automatically overridden to 0, and APPLICATION_FILE was updated to #include "test.h".

after_import.png
7. Details of my custom PDO configuration in the Excel file, where Device Profile is configured as 402 with CiA 402-compliant object dictionary entries.

obj_excel.png

Could you advise on the correct workflow to define custom PDOs via an Excel file without having SSC Tool force CiA402_SAMPLE_APPLICATION back to 0?

Environment Information:

  • SoC/Board: AM2612

  • SDK Version: ind_comms_sdk_am261x_2026_00_00_06

  • Tool Version: Beckhoff SSC Tool v1.5.3.0

Thank you for your assistance.