Part Number: AM2434
Hello,
I'm trying to follow the guide here for scripting initialization of AM243x with the ccs scripting console:
Has anyone done this with CCS Theia based CCS? Here is my scripting console output:
js:> loadFile "C:/ti/mcu_plus_sdk_am243x_11_01_00_19/tools/ccs_load/am243x/load_dmsc_hsfs.js"
loadFile "C:/ti/mcu_plus_sdk_am243x_11_01_00_19/tools/ccs_load/am243x/load_dmsc_hsfs.js"
^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^^
Uncaught SyntaxError: Unexpected string
js:>
I am using CCS 21.00, and I know this is an older version of the SDK, but I would expect it to work much the same since the script itself probably hasn't changed...
Note that there is no "loadJSFile" command in the CCS21 scripting console which is why I used the loadFile command.
Munan