This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: sysconfig regression for importing flash json configurations.

Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG

Hello,

I have a customer using the latest AM243x SDK (12_00_00_27) and it defaults to sysconfig 1.26 in the project settings.

Using sysconfig 1.26 you can import a flash config from JSON and it updates the values in the flash driver accordingly.

However, if you change the project settings to sysconfig 1.27 then the import breaks:

image.png

image.png

More recent versions of sysconfig also have this issue. Just wanted to note the regression so it can get fixed in subsequent releases.

Munan