This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1106: Configuring ADC not available via SysConfig tool

Part Number: MSPM0G1106
Other Parts Discussed in Thread: SYSCONFIG,

Hi,

I'm looking to use the PA14/18 pin of the MSPM0G1106(32pin config) for ADC reading which doesn't seem possible using the SysConfig tool. Depending on which ADC(0 or 1) I choose, it only allows either the pin PA27 or PA15.

If I wanted to use the PA14 pin for ADC reading through ADC0 channel 12, do I need to directly configure it using the DriverLib APIs?

Is there a better way to go about this situation you would recommend?

image.png

image.png

Thank you,

Kyungjae Lee