This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: AM263P4 SBL26 compiled with SDK26 cannot implement the SWAP function, while SBL11 compiled with SDK11 can implement the SWAP function.

Part Number: AM263P4

I respectively imported the SBL examples (sbl_ospi_swap) from mcu_plus_sdk_am263px_11_00_00_19 and mcu_plus_sdk_am263px_26_00_00_06, and only the following modifications were made to the two projects:

image.png

Test description: The BOOT has been switched to SDK26. The SWAP flag is modified via Flash operations (address 0x60080080–0x60080083), where 0x5A5A5A5AU represents Bank B and 0xA5A5A5A5U represents Bank A. Both SBLs use the same BOOT.AM263P4 is HS_SE

For the sbl_ospi_swap example from mcu_plus_sdk_am263px_11_00_00_19:
Phenomenon: The SBL can successfully achieve A/B bank switching according to the SWAP flag: SBL detects the flag set to Bank A -> jumps to the BOOT in Bank A -> the BOOT modifies the flag to Bank B -> power cycle -> SBL detects the flag set to Bank B -> jumps to the BOOT in Bank B -> the BOOT modifies the flag to Bank A -> and the cycle repeats.

image.png

For the sbl_ospi_swap example from mcu_plus_sdk_am263px_26_00_00_06:
Phenomenon: The SBL cannot achieve A/B bank switching according to the SWAP flag: SBL detects the flag set to Bank A -> jumps to the BOOT in Bank A -> the BOOT modifies the flag to Bank B -> power cycle -> SBL detects the flag set to Bank B -> still jumps to the BOOT in Bank A -> the BOOT modifies the flag to Bank B -> and the cycle repeats.

image.png