This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: SWD mode with XDS100v3

Part Number: MSPM0G3507

Hi Champ,

I am asking for my customer.

They had few XDS100v3 debug tool left for previous design with other MCUs.

They are asking whether XDS100v3 could support and program our M0 devices.

They had tried to select the XDS100v3 for Connection column at Basic page in .ccxml file. However, we don't see a place where we could select JTAG/SWD/cJTAG as selecting XDS110 for connection at Advanced page.
Therefore, we tried with the Generate 1149.7 2-pin advanced modes for the converter usage and kept other columns as original default. However, pressing Test Connection, it showed the error as below.

IMG_0003.jpeg

We would like to ask if XDS100v3 could support MSPM0 devices? If so, what's the configuration in .ccxml file? Please explicitly show us the setup.

Thanks for the support.

Regards,

Johnny

  • Hi Johnny,

    The XDS100v3 cannot be used to debug or program the MSPM0G3507 through its normal debug interface. The MSPM0G3507 uses the ARM Serial Wire Debug (SWD) interface, while the XDS100v3 does not support SWD. Its available debug modes are JTAG and cJTAG/IEEE 1149.7. Therefore, the “Generate 1149.7 2-pin advanced modes” option is not equivalent to SWD; 2-pin cJTAG and SWD are different protocols.

    This is also why CCS does not provide the same JTAG/SWD/cJTAG selection when XDS100v3 is chosen that you see when using an XDS110. The connection failure shown in your test is consistent with attempting to access an SWD target using an unsupported XDS100v3 signaling mode.

    For the MSPM0G3507, I recommend using an XDS110 or another debug probe that explicitly supports ARM SWD. In the CCS target configuration, select the Texas Instruments XDS110 USB Debug Probe, select MSPM0G3507 as the device, and configure the connection for SWD. The physical connection should include SWDIO, SWCLK, GND, target voltage reference, and preferably NRST.

    Unfortunately, there is no .ccxml setting that can make the XDS100v3 operate as an SWD probe for the MSPM0G3507. The absence of an SWD option when XDS100v3 is selected is expected and is not a CCS configuration issue.

    Regards,
    Brian