This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2732-Q1: AM2732-Q1 external clock specifications

Part Number: AM2732-Q1
Other Parts Discussed in Thread: AM2732

Hello,

at datasheet of AM273x there are extremely strict requirements regarding the phase noise of the external clock.

We are not intending to use the AM2732 for radar applications or distribute the clock to other devices for having coherency. Clock will be used only for AM2732's internal phys (ethernet, lvds, qspi and csi-2). 

Are the phase requirements also need to be met in this scenario?

 

Thank you for your time.

Konstantinos

  

  • Hello Konstantinos,

    The strict phase noise requirements specified in the datasheet are not necessary for your use case. Those specs are targeted at users leveraging the AM273x's radar front-end capabilities (APLL, RF synthesizer, and cascaded coherent configurations). The phase noise specifications in the AM273x datasheet are primarily driven by the radar RF synthesizer, specifically the APLL (Analog PLL) used by the radar front-end subsystem. Phase noise on the reference clock directly translates to phase noise on the synthesized RF carrier, which critically degrades Doppler resolution and radar sensitivity.

    Since you are not using the AM2732 for radar processing or cascaded front-end coherency, several points apply:

    • QSPI (up to 67 MHz) — This is a relatively low-speed, synchronous digital interface. Its timing is governed by the digital PLL output, not by the raw reference clock phase noise. The requirements here are very relaxed.
    • Ethernet (10/100 Mbps RGMII/RMII/MII) — The Ethernet MAC/PHY generates its own recovered clock and uses standard Ethernet signaling tolerances. Phase noise of the source reference clock has negligible impact at these speeds.
    • LVDS (Aurora TX, up to 900 Mbps/lane) — The LVDS interface on the AM273x is a TX-only interface used to output radar ADC data to external instrumentation. Its clock is derived from the device's internal digital PLL. While high-speed serial interfaces are more sensitive to jitter than low-speed ones, the tolerance here is far less stringent than for a radar RF synthesizer.
    • CSI-2 (MIPI D-PHY, up to 1 Gbps/lane) — CSI-2 uses embedded clock signaling (data and clock are correlated), so the source reference clock quality has minimal impact on link integrity.

    Best Regards,

    Borislav Lazarkov

  • Hello Borislav,

    thank you for the prompt and detailed response.

    Kind regards,

    Konstantinos Lekkas