Hi.
I'm using RM48HDK and Spectrum Digtla XDS560v2, CCS4.2
So, I'm trying to connect RM48HDK with system trace function.
How can I use it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I'm using RM48HDK and Spectrum Digtla XDS560v2, CCS4.2
So, I'm trying to connect RM48HDK with system trace function.
How can I use it?
Hello,
MIPI STM system trace is not supported on the RM48 hardware. The RM48 hardware supports the industry standard ARM ETM (embedded trace macrocell) for CPU trace and the proprietary RTP interface for ram trace. Tools are available from Lauterbach and Vector to support these interfaces.
Regards,
Karl