Other Parts Discussed in Thread: RM48L950
Hello all
I am working on a programable Laser control board for a laser projector.
The way I see this working is like this..
This control board will have a MCU's that reads the analog input signal and adjusts a digital pot on the Adjust pin of a LM350,, so it will adjust the out put power to a laser.
The user interface should give a choice of 1 or 4 analog read signels per color,, for now we only are looking at two colors Red and Blue.
This is the single analog input per color idea,,, I need to control 4 red and 4 blue and the way I see this happining the first red Laser begins to lase at a set analog input level say 0.35V and as the wave reaches say 1.35V the second red laser lases,,, as the wave reaches reaches its peak 5V all 4 come up to the full preset user interface value.
Here is the second user interface choice,,, multi analog read,,, each analog signal controles its own Laser to its preset user interface value.
The MCU I have is the RM48L950 and it has 54 I/O ports which 48 are used control 8 TPL8002-25PWR,, will their still be enough to add a digital display with a user interface control? I mean their is only 6 I/O ports and 8 analoge ports left?
Is their a downloadable autocad foot print?¿ Even better is their a down loadable,, general foil pattern for the RM48L950 that I can mod?¿
is their a basic schemadic for it?
Thanks Jeff.