This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: MSPM0C1104 Password-Protected Debug Demo Project and DSSM Documentation

Part Number: MSPM0C1104
Other Parts Discussed in Thread: UNIFLASH

Hello,

I'm evaluating the software-based password-protected debug approach described in this application note: Realization of Password-Protected Debug Based on Software. The document references demo code and CCS scripts for implementing password-protected debug via DSSM and SEC-AP.
 
However, I have not been able to find these resources anywhere.
The note states:
"TI has provided the code project and CCS scripts which have the demo code to achieve password-protected debug function."

Are the demo project, GEL scripts, and CCS examples publicly available? If so, where can they be found?

I also have some questions regarding the DSSM (Debug Subsystem Mailbox):

  • Is there any public documentation describing the DSSM protocol, command set, mailbox register map, or SEC-AP access sequence?
  • Can DSSM be accessed from third-party SWD tools such as SEGGER J-Link, or is it intended only for CCS/XDS110?
  • Are there any examples showing DSSM communication without CCS?
My goal is to implement a custom password-authentication and firmware update workflow using SWD and J-Link, so I'd like to understand whether DSSM can be used independently of the tools provided by TI and what documentation is available.
 
Thank you for any guidance.
 
Best regards,
Lukas