Part Number: MSPM0C1103
Hi srs,
We are using the MSPM0C1103 microcontroller to read two ADC ports.
However, we have identified an operational stability issue.
In a batch of 200 units, 60% function correctly, while 40% experience an application freeze when reading the second ADC port.
The firmware is identical across all units. We have also determined that this freezing issue in the 40% of units occurs only when reading more than one ADC port; if we modify the firmware to read from a single ADC port, the microcontrollers function correctly in 100% of cases.
The firmware is quite simple and follows standard recommendations, yet it still works on only 60% of the chips.
Part of the code follows below.
#include "ti_msp_dl_config.h"
volatile uint32_t Timer_REM_TX = 0, Timer_falha = 0, Timer_Bit = 0;
volatile bool gCheckADC = 0;
uint16_t gAdcResultFinal[2] = {0,0};
int main(void)
{
SYSCFG_DL_init();
NVIC_EnableIRQ(TIMER_0_INST_INT_IRQN);
DL_TimerA_startCounter(TIMER_0_INST);
NVIC_EnableIRQ(TIMER_1_INST_INT_IRQN);
DL_TimerG_startCounter(TIMER_1_INST);
DL_GPIO_setPins(GPIOA, TX_MED_PIN_11_PIN);
DL_ADC12_startConversion(ADC12_0_INST);
while (1) {
// Aguarda a conversão anterior terminar via polling de hardware
while (!(DL_ADC12_getRawInterruptStatus(ADC12_0_INST, DL_ADC12_INTERRUPT_MEM1_RESULT_LOADED)));
gAdcResultFinal[0] = DL_ADC12_getMemResult(ADC12_0_INST, DL_ADC12_MEM_IDX_0);
gAdcResultFinal[1] = DL_ADC12_getMemResult(ADC12_0_INST, DL_ADC12_MEM_IDX_1);
.....
}
}