Part Number: TM4C1294KCPDT
Other Parts Discussed in Thread: MAX3221
Hi,
I have a customer attempting to program a custom TM4C1294KCPDT board via UART.
They have reported the following error:

I have confirmed the following:
- They are able to program via JTAG
- They are unable program empty MCUs via UART
- Their RS232 circuit is connected to UART0
- MAX3221 transceiver is used
- RBIAS is present
- They have confirmed sucessful data reception with the RS232 circuit using a monitoring tool