This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751: TPS25751 Read opponent PID/VID error ananlysis

Part Number: TPS25751

To read the PID/VID information of the opponent from the TPS25751, is it done through the 0x48h register?

If all values ​​read are 0, are there any other prerequisites for correct reading?

If not, which register should be read to determine the counterpart's PID/VID?
  

  • Hi, 

    Thanks for reaching out on E2E. Register 0x48 is not the correct register, you will want to read from register 0x47 for the PID/VID.

  • Hi Jason,

    can you provide table to explain each bit for 0x47 register?
    I've dump 0x47 register as following, but i do not know what it means

    [00:45:51.285,766] <inf> ti_tps25751: [tps25751_dump_reg] 0x47 len=25 (26 bytes)
    [00:45:51.285,797] <inf> ti_tps25751: [dump_reg] [00] 19 04 51 04 40 50 00 00 00 00 11 09 40 00 40 00
    [00:45:51.285,858] <inf> ti_tps25751: [dump_reg] [16] 00 61 00 00 00 00 00 00 00 43

  • Hi,

    Sorry about that I made a mistake.

    For your issue if you are needing to differentiate between different TPS25751 PD controllers. You can use the "Customer_Use" register (0x06). You may enter any 64bit value into this register to differentiate between PD controllers.

    Or is specifically the PID/VID what you are needing?

  • Hi Jason,

    Thanks, but let me clarify — what I need is specifically the VID/PID of the attached port partner (the device plugged into the TPS25751's Type-C port).

    Thanks,
    Kevin

  • Hi Kevin,

    Ok understood. 

    Sorry about the earlier response I was mistaken register 0x48 is the correct register.

    This register is populated after a Discover Identity command is sent to the port partner and is ACK'd