This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1306: Configure the L1306 clock to 16MHz

Part Number: MSPM0L1306

Hi experts,

I would like to configure the L1306's MCLK to 16 MHz for a UART application.

image.png

image.png

However, it failed the FCC inspection.

Any suggestions for this issue?

Thanks

  • Hi Leo,

    I will recommend to use clock tree to configure the SYSOSC user trim function. But there are some modification required to make the function work:

    1. Enable SYSOSC user trim function.

    2. Configure FCC function. (trigger clock: LFCLK, FCC clock: SYSOSC) 

    3. Modify the order of FCC configuration and SYSOSC user trim configuration in SYSCFG_DL_SYSCTL_init() API. (make sure FCC is enabled and configure before user trim)

    I uploaded an example based on M0L1306 for your reference: empty_LP_MSPM0L1306_nortos_ticlang_usertrim_16MHz.zip