Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS31 Hercules HDK and Keil Software

Good Afternoon,

I recently purchased a TMS570LS31 Hercules HDK board, and would like to use the KEIL IDE with it. I have tried to connect through the USB port, which will connect to the demo software which came with the board, but with no success. Do you need to use one of the JTAG interfaces, and if so what other hardware would you need to connect to a USB port? Does TI make such a module?

Any help would be appreciated.