AM263P4-Q1: Regarding the "[HSM_CLIENT] Timeout exception”

Part Number: AM263P4-Q1

We are currently migrating from SDK 9.02 to SDK 11.0.

During startup, we use the following APIs to configure the firewall:
HsmClient_register
HsmClient_setFirewall

At that time, the following error log is generated:
[HSM_CLIENT] Timeout exception
This error log was not generated when using SDK 9.02.

What could be causing this error after migrating to SDK 11.0?

Requested response date: September 15, 2026

  • Hi Atsuki san,

    Which TIFS version are you using along with SDK 11.0 ?

    Also, which memory regions are you trying to firewall which are giving a timeout?

    Thanks and Regards,
    Aditya Singal

  • To check the TIFS version, we tried to obtain it using HsmClient_getVersion(), but SystemP_TIMEOUT is returned, and we are unable to get the version.


    Is there any other way to check the TIFS version?


    Also, if there is a possibility that the HSM is not starting up or operating properly in the first place, could you please advise us on the procedure to check the operating status of the HSM?


    The memory regions we are trying to firewall are the OCSRAM (Bank0 to Bank3) and the FLASH region.


    Requested response date: October 2, 2026

  • Hi,

    From the above explanation, it looks like the device has not booted the HSM firmware as none of the services are being acknowledged.

    What is the status of the loadHSMFirmware API in your bootloader? Did you get the boot notify from HSM there?

    Thanks and Regards,

    Nikhil Dasan

  • Hi Nikhil

    HsmClient_loadHSMRtFirmware(), which is called from Bootloader_socLoadHsmRtFw() in the bootloader, returns SystemP_SUCCESS.
    Within HsmClient_loadHSMRtFirmware(), the following code waits for a boot notification from the HSM. Since the subsequent processing continues successfully, we believe that the HSM boot notification has been received and that the HSM firmware has started correctly.

    status = HsmClient_waitForBootNotify(NotifyClient, SystemP_WAIT_FOREVER);

    Could you please advise if there are any other points that we should check?

    Requested response date: October 6, 2026

  • Hi,

    Are you running this on HS-SE device? 

    If yes, then you can open the debug for HSM core and check what is happening there.

    If it is HS-FS, then this is not possible as JTAG is locked for M4.
    If that is the case, can you share the screenshot of the log from your end and the code that you are running?

    Thanks and Regards,

    Nikhil Dasan

  • Hi Nikhil

    The following is the log output captured when HsmClient_getVersion() was executed in the environment prior to the migration to SDK 11.0.
    Based on this result, we understand that the application was running on an HS-FS device.

    We would also like to provide one additional clarification.
    Although we are currently migrating to SDK 11.0, the SDK versions on which the original images are based are as follows:

    - Loader image: Based on SDK 10.0
    - Application image: Based on SDK 9.02

    We will share the screenshot of the log captured when the issue occurred, along with the relevant code, via email.
    We would appreciate your cooperation in analyzing this issue.

    Requested response date: October 12, 2026

  • Sure, awaiting your package over mail. 

    Meanwhile, in the screenshot, I see that the version used for HSMRT is 10.0. Are you migrating to 11.0 keeping hsmrt of 10.0? 
    Please use the hsmrt of 11.0 as well

    Thanks and Regards,

    Nikhil Dasan

  • Hi Nikhil

    We have requested that the log screenshots and related code be sent to you.
    If you have not received them yet, please let us know.

    Also, we would appreciate it if you could let us know when you expect to be able to share the analysis results.

    > Meanwhile, in the screenshot, I see that the version used for HSMRT is 10.0. Are you migrating to 11.0 keeping hsmrt of 10.0?

    This screenshot was taken in the pre-migration environment.
    In the post-migration environment, HSMRT version 11.0 is being used.

    Currently, in this post-migration environment, the HSM-related APIs are returning SystemP_TIMEOUT, and we are also unable to retrieve the HSMRT version information.

    Requested response date: October 19, 2026

    Imada

  • Hi Imada-san,

    I've received the package. Let me check and get back to you.

    Thanks and Regards,

    Nikhil Dasan

  • Hi Nikhil,

    Hello.

    It has been over a week since my previous message. Could you please let me know the current status of this matter?

    This issue is also a high-priority matter on our side.

    Therefore, I would appreciate it if you could provide a response by the end of today (October 28, 2026) or tomorrow (October 29, 2026).

    Thank you for your cooperation.

    Best regards,
    Imada

  • Hi Imada-san,

    Apologies for the delay.

    I was trying to get the SBL and APP build and run at my end. The App didn't run due to some ADC dependency. 

    So I added the  HsmClient_getVersion in the bootloader itself after HSM loading and I was able to get the correct version for the HSM

     
     #define CLIENT_ID                               (0x02U)
    
    /* 
        Size of buffer which stores the parsed version 
        from the reponse received from HSM.
    */
    #define PARSED_VERSION_BUFFER_LENGTH            (0x96U)
     
     
     
     
        char parsedVer[PARSED_VERSION_BUFFER_LENGTH];
        HsmClient_t client;
        HsmVer_t hsmVer;
        
        status = HsmClient_register(&client, CLIENT_ID);
    
           /* Send Request for TIFS-MCU version to HSM Server */
        status = HsmClient_getVersion(&client, &hsmVer,5);
        DebugP_log("[HSM CLIENT] HsmClient_getVersion() status = %d\r\n",status);
    
        DebugP_log("[HSM CLIENT] OTP-KW 64bit version string = 0x00%llx\r\n",hsmVer.HsmrtVer);
        DebugP_log("\r\n [HSM CLIENT] OTP-KW Information");
        status = HsmClient_parseVersion(&hsmVer, parsedVer);
        DebugP_log("%s\n\r", parsedVer);

    Have you tried the same at the bootloader side? Could you let me know the result at your end with this test?

    The screenshot shared had only logs from Application. 

    Can you share your bootloader logs to show that HSM has loaded correctly?

    Thanks and Regards,

    Nikhil Dasan

  • Hi Nikhil,

    Thank you for your confirmation.

    In our environment, we also called HsmClient_register() and HsmClient_getVersion() on the SBL side after loading the HSM. Both functions completed successfully, and we confirmed that the HSM version could be retrieved. Please find the SBL log below.

    On the application side, however, as shown in the screenshot shared previously, the HSM-related APIs return SystemP_TIMEOUT, and the HSM version cannot be retrieved.

    Additionally, we identified a separate issue with an ADC dependency that had prevented the application from running. This issue has now been fixed. We will also provide the updated source code.

    We would appreciate your continued assistance in investigating why the HSM-related APIs return SystemP_TIMEOUT in the application.

    Requested response date: November 3, 2026

    Imada

  • Thank you for the confirmation and letting me know that hsm services works fine in bootloader. This confirms HSM is loaded successfully. Please share me the updated application code so that I check the same at my end.

  • Hi Nikhil,

    I understand that this issue was shared internally by Mr. Morita from Texas Instruments Japan on November 2, 2026.

    However, we have not received any update since then. As this issue remains a high-priority matter on our side, we would appreciate an update on the current investigation status.

    Could you please let us know the current status and any findings available at this point?

    We would appreciate receiving your response by tomorrow (November 11, 2026) or the day after tomorrow (November 12, 2026).

    Thank you for your cooperation.

    Best regards,
    Imada

  • Hi Imada-san

    Apologies for the delay due to festival holidays in India.

    In your project, please change the MPU region as shown below to Shareable.

    This is because, the variables in RAM in a service would be accessed by HSM as well, so this is needed for that region

    With this I see getversion and setFirewall passing.

    Thanks and Regards,

    Nikhil Dasan