Part Number: AM2434
Other Parts Discussed in Thread: SYSCONFIG
Hello,
currently I am migrating my project from SDK v11.00.00 to v2025.00.00 and one of the modules / drivers i am using is SDFM. I went through the migration guide and the sample projects, and was able to successfully update my project to the new driver API. However, I have observed some strange behavior. Suddenly, there is a large offset in the SDFM module.
To summarize briefly: When SDFM is configured, for example, to use a SINC3 with an OSR of 64 (Value range: 262144), the raw sample value for no current should be 131072. However, the driver returns raw sample values of approximately 126000. When I calculate current values based on the hardware (shunt resistor), the linearity of the current values however is correct. If the power supply e.g. is set to 1A, 5A, 10A the raw sample value (or the calculated current) is correct, but it is shifted by the offset.
I did not experience this behavior with the older version of the SDFM drivers/firmware. Is this a known issue, or am I missing a configuration step in the new driver/firmware architecture?
Best regards,
Christian