Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: Regarding microcontroller selection and life cycle for new design

Part Number: TMS570LC4357-EP

Dear Team,

Could you please confirm which microcontroller is more suitable for MIL grade Airborne application, Life cycle, latest and advanced technology among following

  1. TMS5704357BGWTEP
  2. TMS5703137CGWTMEP

Also confirm whether it will be availble for next 15 years.

 

  • The TMS5704357BGWTEP is the newer of the 2 devices, using a ARM Cortex R5F(400MHz), vs a R4F(300MHz) on the other device, as well as latest peripherals.  They are both manufactured in the 65nm Flash process node.

    I would refer you to our product lifetime policy https://www.ti.com/quality-reliability/quality/product-life-cycle.html, essentially there are many milestones that must be met for TI to discontinue a device, especially since these are both EP devices.

    With that said I would go with the 4357, as it has a newer intro date and has a superior CPU core vs the 3137.  

    In terms of applicability to MIL grade Airborne applications; I know the -55C that both devices have is helpful here, both have lead solder balls which I believe is also desirable for avionics. 

    Best,

    Matthew

  • When this microcontroller TMS5704357BGWTEP came in market?
    and when we click on the lifetime policy it is telling in Active state but nowhere it is mentioned that it will be available fir next 15 years atleast. Kindly confirm the lifecycle? Or confirm if we can use this TMS5704357BGWTEP in our new design.?

  • This device was released in May of 2018.  For future reference you can look in a device DS upper right corner, https://www.ti.com/lit/ds/symlink/tms570lc4357-ep.pdf It will have an intro date and date of latest revision.

    The key for lifetime on the link I sent is that if the device had any sales within the last 7 years(for EP) or any current customers then a device is not eligible for obsolescence.  So, if you decide to move forward with a design based on this device, and order it, TI will not obsolete it unless either of the above 2 conditions are met.

    If this device was scheduled for obsolescence or already obsolete there would be a banner on the product folder indicating this.

    You can use this for your new design.

    Best,

    Matthew