Part Number: AM2612
Other Parts Discussed in Thread: SYSCONFIG, LP-AM261, DP83826E
Hello TI Team,
We are developing a custom AM2612 board based on the Industrial Communications SDK PROFINET Device example.
The current PROFINET Device example is configured to use ICSSM0. In our current Custom SysConfig configuration, PROFINET uses ICSSM0, while General Ethernet / ICSS-EMAC uses ICSSM1.
For our final custom board architecture, we are considering moving the PROFINET Device application from ICSSM0 to ICSSM1. We would also like to evaluate the ZEJ package for a future production board because of PCB area and pin-assignment constraints.
Could you please clarify the following?
- PROFINET on ICSSM1
- Is the current use of ICSSM0 in the PROFINET Device example only due to TI validation coverage, or is the PROFINET firmware/FWHAL architecture functionally tied to ICSSM0?
- Is it technically possible to run the PROFINET Device application on ICSSM1?
- If supported, what changes are required for migration from ICSSM0 to ICSSM1?
- SysConfig configuration
- Board and pinmux configuration
- Generated source files
- Interrupt and event mapping
- FWHAL configuration
- PROFINET stack adaptation
- PRU firmware selection or build configuration
- Does TI officially support and validate PROFINET Device operation on ICSSM1, including 2-port operation? If not, please clarify whether this would be considered a customer-owned implementation.
- ZEJ package support for 2-port PROFINET Device
We have already completed basic PROFINET testing using the LP-AM261 platform. For the production board, we are considering the AM2612 ZEJ package.
Could you please confirm:
- Are there any known limitations when implementing a 2-port PROFINET Device with the ZEJ package?
- Are there any mandatory ICSSM/PROFINET signals available on ZCZ but unavailable on ZEJ?
- Which ICSSM instance, ICSSM0 or ICSSM1, is recommended for a 2-port PROFINET Device design using the ZEJ package?
- Does TI provide a recommended pin assignment, pinmux example, reference design, or validated custom-board configuration for ZEJ package based 2-port PROFINET?
- Are there additional restrictions related to Ethernet PHY reset, MDIO, reference clock, interrupt/event routing, or PRU-ICSS pin assignment when using ZEJ?
Our goal is to build a custom 2-port PROFINET Device board using the actual ZCZ or ZEJ package pin assignment, rather than retaining the LP-AM261 board configuration.
Thank you for your guidance.
Best Regards,
Jack Cha