This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: CAN based FBL (bootloader) for MSPM0

Part Number: MSPM0G3507

Hello TI Team,

We are currently working on an automotive ECU project using the MSPM0 [MSPM0G3507] controller.

We require a bootloader solution to perform application firmware updates over CAN. Could you please provide a demo/reference implementation for a CAN-based bootloader for the MSPM0 family, if available?

Our preliminary requirements are:

MCU: MSPM0 [MSPM0G3507]
Interface: CAN
Flashing protocol: [UDS/ISO-TP or proprietary CAN protocol]
Bootloader should support Flash erase and programming
Bootloader-to-application jump
Recovery/handling of interrupted firmware updates
Development environment: [CCS] with MSPM0 SDK [  2.10.00.04]