Part Number: AM2612
Other Parts Discussed in Thread: MCU-PLUS-SDK-AM261X
We are implementing functional safety diagnostics on the AM261x using the ECC/SDL functionality provided in motor_control_sdk_am261x_10_02_00_07.
We would like to confirm whether ECC diagnostics can be performed for the VIM (Vectored Interrupt Manager).
Specifically, we would like clarification on the following points:
- Is the VIM RAM on the AM261x protected by ECC?
- Is the VIM RAM protected by an ECC mechanism such as SEC/DED?
- Is it possible to intentionally inject a single-bit or double-bit error into the VIM RAM in order to verify the ECC diagnostic functionality?
- Does the SDL in Motor Control SDK 10.02.00.07 support VIM ECC self-test or error injection?
- Is there an API or example code in the SDK for performing ECC diagnostics on the VIM?
- Can the VIM be specified as a target memory/module through SDL_ECC or other ECC-related SDL APIs?
- If SDL_ECC does not support VIM ECC diagnostics, is there another recommended method for performing an ECC self-test or error injection for the VIM?
- Are injected VIM ECC errors reported to the ESM?
If a VIM ECC error is intentionally injected, is the detected error reported to the ESM?
We would like to know the corresponding ESM Event / Group / Bit Number, if applicable, for each of the following:
- Single-bit ECC error
- Double-bit ECC error
If VIM ECC error injection or self-test requires any additional configuration or a specific procedure, could you please provide the recommended method?
Best Regards