This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1228: attach to running application in IAR

Part Number: MSPM0L1228

Hello,

Is there a way to attach to a running application without reset in IAR? 

There is no option for no reset in the TI XDS settings (ignore the project name it's the same for any of the M0's):

image.png

Munan

  • Hey Munan,

    switching from the TI XDS110 settings to the CMSIS DAP, will allow you to connect without a reset:

    The following was captured after power cycling the board and using the Project->Attach to running target option:



    Best Regards,
    Brian