Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: information about external sync in configuration for EPWM

Part Number: AM6442
Other Parts Discussed in Thread: AM263P4

I am trying to create 8 independent PWM with external sync in for am6442 and am263p4. But datasheet says it has only 3 (am6442) and 2 (am263p4).

please confirm this

  • Hello Harshad,

    Thank you for your query !

    Let me check and confirm.

    I will follow-up later today.

    Thank you

    Best Regards,

    Anastas Yordanov

  • Hello Harshad,

    Thank you for your query !

    As I checked I can confirm that in the AM6442 there are  9 x EPWM modules (EPWM0 - EPWM8). Indeed, ONLY 3 of them - the EPWM0, EPWM3 and EPWM6 have their SYNCI input and  SYNCO output mapped to AM6442 SoC level pins.

    This can be seen in the AM64x/AM243x TRM / Chapter, PEripherals/Section, Industrial And Control Interfaces / Section, EPWM / Section, EPWM Environment/ Section, Daisy-Chain Connectivity between EPWM Modules

    As far as I can see in the AM263Px Datasheet and AM263Px TRM, there are 32 EPWM modules with EPWM outputs integrated. I am not familiar with the actual mapping of AM263Px internal sync sources to the EPWMj.SYNCI inputs and EPWMj.SYNCO (j=0..31) to output signals inside AM263Px, as there is an EPWM dedicated crossbar used. The AM263Px processor family is  a non-AM6x SITARA processors family and is supported by a different TI E2E unit than SITARA PROCESSORS. I will recommend you to contact them to confirm. Therefore I will forward your request to them to further clarify and help you. 

    Thank you !

    Best Regards,

    Anastas Yordanov

  • Hello,

    As for AM263P, all ePWMs have sync out source. you can simply enable one sync out in any ePWM and use it as the source for all "sync in" in the other ePWMs.

    Best Regards,

    Masoud