Part Number: AM2632-Q1
Hi team,
I ask this for my customer
1.If the crystal oscillator (XTAL) stops working on the AM263, can the SOC still receive an external WARMRSTn signal from an external watchdog? can AM263 be reset by WARMRST signal?
2. If the crystal oscillator (XTAL) stops working on the AM263, what will be the state of each IO pin on the SOC? Will the output pins hold their last driven state, go Hi-Z, or be pulled to a default level? Does the behavior differ between output pins, input pins, and bidirectional pins?
3. Does triggering a Warm Reset (via WARMRSTn) require the crystal oscillator (XTAL) to be functional? If the XTAL is not working when a Warm Reset is triggered, will the SOC be able to complete the reset sequence and exit reset normally? And what state will the IO pins be left in if the SOC cannot exit reset due to the absence of a clock?
4. This has a max timing requirment for WARMRST, if the external watchdog give longer WARMRST signal(> 16384000 ns) and then pull up the WARMRST signal, what will happen? can device release from reset?

BRs
Shuqing