Part Number: AM263P4-Q1
Hi Team ,
For checking successful completion of pbist positive test for each memory region, Is it enough to check FSRF (0x5330 0190h) reg value alone according to SDK code? Since this value is by default 0 and on successful completion also it indicates 0, how are we supposed to know if the test is done and the value zero is due to pbist positive test success.
In the sdk pbist code, we are using something called scramble value SDL_PBIST_InstInfoArray. Are these scramble value written to memory region being tested, when I notice memory browser after positive test, should these scramble value be visible in CCS memory browser?
Thanks & Regards,
Vandana Chintala