Part Number: AM2432
While determining if function Sciclient_waitForMessage will be called, function Sciclient_service of SCICLIENT in MCU+ SDK for processor AM243X v12.01.00.33 checks if any of the bits [0] and [1] of pReqPrm->flags are set. However bit [0] is documented as reserved in macro TISCI_MSG_FLAG_RESERVED0. Why is it checked in function Sciclient_service if it is reserved?