Part Number: MSPM0G5116
Other Parts Discussed in Thread: SYSCONFIG, MSPM0G5187
Hello,
There seems to be an issue with how SysConfig (In CSS version 21) when using TinyUSB and the MSPM0G511x micros.
The first pic shows the selection made in SysConfig
This Picture shows the SysConfig.config file in text
this Pic shows the ti_msp_dl_config.c generated
notice LFCLK is in the code not LFXT - this generates and error undeclared identifier - this line
can not be edited because it is always overwritten at build.
This Pic show SysConfig using SOF (not LFXT)
This Pic again shows the SysConfig in text (no SOF(which maybe default) or LFCLK)
Yet - This Pic shows the generated ti_msp_dl_config.c generated
Still adding the wrong information?? If SOF why this line. Cannot edit because build puts it back.
It is hell bent on adding the LFCLK line.
This Pic show what is used in the dl_sysctl_mspm0g511.h (LFCLK)
Undeclared identifier error from ti_msp_dl_config.c
Am I goofy and just missing something.
With the MSPM0G5187 there appears to be no issue
Thanks Mike