Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

[FAQ] AM2612-Q1: How to use UniFlash CLI Tool

Part Number: AM2612-Q1
Other Parts Discussed in Thread: UNIFLASH

Hi expert, 

Please provide steps to flash AM261 using UniFlash CLI tool.

Provide commands for relevant operations as well

  • Steps to Setup

    Download the uniflash_windows setup from the uniFlash tool.

    Run one_time_setup.bat - Installs the XDS110 / ICDI USB drivers.

    Extract the zip file and save it at a location in your pc.


  • Steps to Erase

    All commands are run from the package folder:

    cd <your-path>\uniflash_windows

    Set the two image paths once (Command Prompt / cmd.exe):

    set SBL=<sdk-instllation-path>/examples/drivers/boot/sbl_ospi_multicore_elf/am261x-lp/r5fss0-0_nortos/ti-arm-clang/sbl_ospi_multicore_elf.release.tiimage
    set APP=<sdk-instllation-path>/examples/hello_world/am261x-lp/r5fss0-0_nortos/ti-arm-clang/hello_world.release.mcelf

    Full erase:
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "EraseActionChoice=Erase entire flash" -b EraseAll

    Erase selected blocks (e.g. blocks 0,1 and 3):
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "EraseActionChoice=Erase specific flash blocks" -s "StandaloneEraseSpecificText=0-1,3" -b EraseBlocks


  • Steps to Flash and Verify

    Flash only (no verify):
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "VerifyAfterProgramLoad=No verification" -f "%SBL%,0x60000000" "%APP%,0x60081000"

    Flash and verify:
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "VerifyAfterProgramLoad=Full verification" -f -v "%SBL%,0x60000000" "%APP%,0x60081000"

    Full erase, flash and verify in ONE command:
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "EraseActionChoice=Erase entire flash" -s "VerifyAfterProgramLoad=Full verification" -b EraseAll -f -v "%SBL%,0x60000000" "%APP%,0x60081000"

    Verify only (compare flash against files, no writing):
    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -s "VerifyAfterProgramLoad=Full verification" -v "%SBL%,0x60000000" "%APP%,0x60081000"

    Flash XIP File as well

    set XIP=<sdk-instllation-path>/examples/hello_world_xip_fss1/am261x-lp/r5fss0-0_nortos/ti-arm-clang/hello_world_xip_fss1.release.mcelf_xip

    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "VerifyAfterProgramLoad=Full verification" -f "%SBL%,0x60000000" "%APP%,0x60081000" "%XIP%,0xE0000000"

  • NOTE: XIP files are flashed at the address 0xE000_0000 address, this is not an actual memory map address, this is actually a placeholder address for the uniflash tool to know that the file is a mcelf_xip file

    To verify XIP segment, we can first take the dump of load segments from the mcelf_xip file, save it as a .bin file and use it to compare the contents written in flash. 


    Verification of XIP file

    1. First flash all the files, SBL, APP and APP_XIP

    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -f "%SBL%,0x60000000" "%APP%,0x60081000" "%XIP%,0xE0000000" 

    2. Convert load segment of the mcelf_xip image into bin

    python .\extract_xip.py "%XIP%" .\

    3. Verify all the files

    set SBL=<sdk-instllation-path>/examples/drivers/boot/sbl_ospi_multicore_elf/am261x-lp/r5fss0-0_nortos/ti-arm-clang/sbl_ospi_multicore_elf.release.tiimage

    set XIP=<sdk-instllation-path>/examples/hello_world_xip_fss1/am261x-lp/r5fss0-0_nortos/ti-arm-clang/hello_world_xip_fss1.release.mcelf_xip

    set APP=<sdk-instllation-path>/examples/hello_world_xip_fss1/am261x-lp/r5fss0-0_nortos/ti-arm-clang/hello_world_xip_fss1.release.mcelf

    set XIP_SEG=C:\Users\Aswin\Downloads\uniflash_windows\xip_seg1_0x60100000.bin

    .\dslite-Cortex_R5_0.bat --mode flash -c user_files/configs/AM261x.ccxml -e -s "VerifyAfterProgramLoad=Full verification" -v "%SBL%,0x60000000" "%APP%,0x60081000" "%XIP_SEG%,0x60100000"

    import struct, sys
    src, outdir = sys.argv[1], sys.argv[2]
    d = open(src, 'rb').read()
    assert d[:4] == b'\x7fELF' and d[4] == 1, "not ELF32"
    phoff, = struct.unpack_from('<I', d, 0x1C)
    phentsize, phnum = struct.unpack_from('<HH', d, 0x2A)
    for i in range(phnum):
        p_type, p_off, p_vaddr, p_paddr, p_filesz, p_memsz, _, _ = struct.unpack_from('<8I', d, phoff + i * phentsize)
        if p_type != 1:  # PT_LOAD
            continue
        flash_off = p_paddr & 0x0FFFFFFF          # same rule as SDK bootloader_uniflash_mcelf.c
        out = f"{outdir}/xip_seg{i}_0x{0x60000000 + flash_off:08X}.bin"
        open(out, 'wb').write(d[p_off:p_off + p_filesz])
        print(f"seg{i}: paddr=0x{p_paddr:08X} size=0x{p_filesz:X} flash_off=0x{flash_off:X} jtag_addr=0x{0x60000000+flash_off:08X} block={flash_off//0x10000}..{(flash_off+p_filesz-1)//0x10000} -> {out}")
    

    The python file is a custom developed python file to extract the load segments from mcelf_xip file and save it as a bin file.