Part Number: AM2434
Is there a method to:
1) Program a new AM2434 throught the EtherNet port or am I to use the USB/emulator route? If so, what is the default IP Address for the new chip?
2) Program the LP-243 Launch Pad without using the USB/Emulator and going through using just the EtherNet port?
If either/or 1) and 2) are possible, is there examples I can use?
Thanks