AM2612: EtherCAT issues when using AM2612

Part Number: AM2612

Hi experts,

when using EC examples, ELCO encountered several issues:

1. Confirm the contents and configuration of the ESC register to facilitate confirmation of whether ESC communication is normal.

2. You need to confirm the configuration of EEPROM in ESI, and whether there is a configuration similar to 9252 regarding device communication and clock lighting.

3. In EC configuration, do the following four pins need to be configured? If so, how should these pins be connected to the external environment?

    

  • Hello Leo Wu,

    On AM261x, the EtherCAT ESC register space for ICSSM0 instance can be accessed at 0x48010000 to 0x48010ED1. Please refer ETHERCAT_SUBDEVICE_CONTROLLER_REGISTER_LIST for register description and recommended default values. The EtherCAT ESC Register Space contains all the EtherCAT-specific functionality

    You can use the EtherCAT Conformance Test Tool (CTT) tool for example to check for the EEPROM configurations.

    3. In EC configuration, do the following four pins need to be configured? If so, how should these pins be connected to the external environment?

    These pin configurations are optional. Please refer to the Hardware_Requirements. 

    Kindly let us know version of the Industrial Communications SDK, the EtherCAT SubDevice example and the hardware type (custom hardware/AM261x LP) you are testing with. Also, please describe the behavior of the SubDevice on the EtherCAT network due to the issues that you are encountered.

    Regards,

  • Hi,

    I have closed this ticket as there is a new duplicated ticket.

    Kind Regards,