Part Number: AM2612
Other Parts Discussed in Thread: SYSCONFIG,
Hi,
TI recommands to start new project from example in communication SDK to use peripheral like ethercat in sysconfig and to start from exemple in motor SDK to use peripheral like endat.
But how is it possible to have a sysconfig with peripheral from both communication and motor SDKs?
In future I will also need system projet to use both core of AM2612. System example projects are in MCU+ SDK.
How to have dual core project + EtherCAT + endat?
Editing syscfg file to add products in header is not enough, as sysconfig seems to search only in folder of the original example project
* @cliArgs --device "AM261x_ZEJ_500" --part "AM2612" --package "ZEJ"--context "r5fss0-0" --product "MOTOR_CONTROL_SDK_AM261x@2025.00.00" --product "INDUSTRIAL_COMMUNICATIONS_SDK_AM261x@2026.00.00" --product "MCU_PLUS_SDK_AM261x@26.01.00"
* @v2CliArgs --device "AM2612" --package "NFBGA (ZEJ)" --variant "500MHz" --context "r5fss0-0" --product "MOTOR_CONTROL_SDK_AM261x@2025.00.00" --product "INDUSTRIAL_COMMUNICATIONS_SDK_AM261x@2026.00.00" --product "MCU_PLUS_SDK_AM261x@26.01.00"
* @versions {"tool":"1.28.2+4845"}
Thanks