Part Number: AM13E23019
Hi Team,
I've had a customer ask after the FLASH subsystem, and want to have clarification on how the Read Interface differs from the Flash Read Interface (FRI) in function, and scope with regards to the ECC for DMA read access.
A related question is on using the FRI-x
The AM13E230x TRM, is unclear in some wording between sections 13.5 - Flash Read Interface and 13.6 - Read Interface, specifically with respects to ECC via DMA access.
Section 13.5.5 indicates ECC doesn't apply to DMA transferred data, but section 13.6.2.1 indicates DMA is protected for single bit errors (provided it's not all 1 or 0).
The intended application is to do flash writes for firmware updating and data storage.
Per current wording for these two cases of how DMA could have ECC, they are contradictory.
Simple ask is there DMA protection; which of these two instances are true?
This ties into the application case - aim is to perform FLASH writes for firmware updating and data storage.
Section 13.5.6 - Procedure to Change Flash Read Interface Registers provides a prescriptive procedure for reconfiguring the FLASH peripheral, which would be undertaken to disable data caching before write.
It's unclear how to route FLASH access through the provided FRI-1/FRI-3/FRI-4 sections, ties into the above question given ECC is needed.
I would understand that to be only viable - if ECC is needed via the CPU data read through FRI-3 (or the others).