Part Number: MSPM0G3519
Hello all,
I have encountered an ECC double bit error in the dataflash region which is causing continous reset.
I noticed a statement in the FEE User Guide: "The system integrator shall add hooks into the NMI handler to ignore any NMI faults generated from the regions dedicated to the FEE module. NMI can happen on reset scenarios when the FEE algorithm attempts to read some corrupted ECC flash region"

- Does this mean TI recommends disabling or ignoring ECC errors for the FEE region?
- What is the risk of keeping it enabled? Is the ECC reporting misleading errors in the dataflash (FEE) region?
- Is disabling the configuration "FEE_USE_ECC_ADDRESS_SPACE" enough or there are other errors which trigger NMI handler that are recommended to ignore/disable (ex: RAM ECC)?
- Regarding the ECC double bit detected on an ECU, is this considered a real error or a fake one and CRC check is enough for the the Fee blocks.