Part Number: MSPM0-SDK
Other Parts Discussed in Thread: MSPM0C1103, SYSCONFIG
I am using CCS12 Version: 12.8.1.00005
I am using the MSPS003F3 variant of the MSPM0C1103 and cannot select resistor pullup under the Digital IOMUX features for an input pin. I also cannot select the digital input filter. I believe this feature was working on an earlier version of the SDK. I can, of course, add my own code with DL_GPIO_initDigitalInputFeatures calls to turn on these features, but it would be nice to be able to use the syscfg interface.
I tried using the Inversion feature on a digital input and found it to work on some pins but not on others. Is this a bug? For example, it did not work on PA4 and PA11.
I have been unable to read back the state of an output pin. There does not seem to be a check box in syscfg to do that. I tried disabling the HiZ parameter in DL_GPIO_initDigitalOutputFeatures but that did not work. Is this even possible?
Thanks,
Tom