Part Number: MSPM33C321A
Other Parts Discussed in Thread: SYSCONFIG
Hi,
with SysConfig [1.28.2-4845] and MSPM33 SDK [V1.04.00.00 ] the generated MCAN initialization (ti_msp_dl_config.c) does not compile:
- The generated code uses the constant
DL_MCAN_FCLK_SYSPLLCLK0, which does not exist in the DriverLib. We assumeDL_MCAN_FCLK_SYSPLLCLKis meant. Patching it manually works, but the fix is lost every time the configuration is regenerated. - The structure
gMCANSYSPLLConfigis generated but never used. A second structuregMCAN0ClockConfis generated and actually used. - The generated code contains the comment
/* Enable MSPM0 MCAN interrupt */. This is only cosmetic, but it raises the question whether the MCAN code generator was fully ported from MSPM0 to MSPM33 and whether generated code and DriverLib really match for this device.
Questions:
- Is this a known issue, and is a fixed SysConfig / SDK release planned? We expected an SDK update around the production release of the device. Is there a release date?
- Until then: what is the recommended workaround that survives regeneration?
Thanks and kind regards