Part Number: TMS570LS0914
Many pins are labeled as low-EMI with a current value. Is that value the maximum current that the pin will source and/or sink? I'm handling latch up possibilities, and if the pins will really only source (when high) and sink (when low) that much current, that simplifies my job a bit.
Also, they are low-EMI pins, but no minimum rise/fall time is given. Are these current-controlled? Is the source impedance specified? I would like to simulate the clock lines on the SPI bus, but I'd need to know the worst case rise time for that.