Part Number: AM263P4-Q1
Hi Team,
I have a couple of questions regarding the OSPI controller initialization and flash reset sequence.
1. OSPI Controller IDLE Bit – Maximum Wait Time
In the OSPI_FLASH_CFG_CONFIG_REG register, the IDLE bit indicates the controller's idle status.
After configuring the OSPI registers, we need to wait until the IDLE bit is set before proceeding with the next operation.
- What is the maximum time required for the controller to set the
IDLEbit after configuring the registers?
- Is there a specified timeout or maximum latency for this bit to transition to 1?
- I would like to avoid using a
whileloop with an arbitrary constant timeout value. Is there a recommended timeout value or a hardware-defined maximum latency that we should consider when polling this bit?
2. Flash Device Reset – Reset Pulse Duration
Regarding the OSPI flash device reset sequence:
- What is the minimum and maximum pulse duration required to assert the flash reset pin?
- How long should the reset pin be held LOW before releasing it (transitioning it back to HIGH)?
- After releasing the reset pin, how much time should we wait before accessing the flash device again?
- Are these timing requirements specific to the flash device, or does TI recommend any standard reset pulse duration?
Could you please provide the recommended timing specifications or point me to the relevant documentation?
Thanks in advance for your support.