AM6422: GPMC configuration question

Part Number: AM6422
Other Parts Discussed in Thread: SYSCONFIG

Hi,

I have a question concerning the GPMC_SYSCONFIG.

There is a IDLEMODE and AUTOIDLE.  what is the effect that if we set "AUTOIDLE" to "0" and "IDLEMODE " to "no idle", we prefer to keep our device constant working. 

  1. But who will send idle request,  definitely it is not the A53, R5F core right?
  2. In which condition will it send idle request?
  3. To keep it constant power, is My configure good?

Thanks.

image.png

  • Hello Jun Tu,
    Are you not using the  MCU+SDK GPMC driver?
    Your Proposed Configuration:
    • AUTOIDLE = 0 (FREERUN)
    • IDLEMODE = NO-IDLE (0x1)
    Effect of This Configuration (Clock Management):
    • GPMC interface clocks remain continuously enabled.
    • There is no automatic internal clock gating.
    • The clock is always supplied to GPMC registers and logic.
    This configuration is correct.
    You are also correct that this is not driven by the A53 or R5F cores executing code.
    The idle request is a hardware-level OCP (Open Core Protocol) initiator-to-target handshake on the interconnect, rather than a register write from a core. 
    Regards,
    Anil