Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

AM6422: SDK8.6 ICSSG1 1Gbit/s

Part Number: AM6422

Hello,

    We have designed our own device that uses one Ethernet port on ICSSG1.With MCU+ SDK 8.6, using the example program, we observe the following:

  • When Ethernet auto-negotiation is used, the link successfully negotiates to 1Gbps, but ping does not work.

  • If we force the port to 100Mbps, ping works normally.

  • If we switch to SDK 11.2, ping works directly at 1Gbps.

So the same hardware works at 1Gbps on SDK 11.2, but fails at 1Gbps on SDK 8.6.

Is this a known issue?

On SDK 8.6, how can we modify or work around this problem? We would like to know how to handle it in both cases:

  1. R5F running FreeRTOS

  2. Linux

Any patches, firmware updates, configuration changes, or recommended workarounds would be appreciated.