Part Number: MSPM0G3519-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hello Together,
We currently facing an issue with the internal temperature sensor and reading the data with Adc channel 11. Currently Vref is enabled with 1,4V and the adc channel is enabled with reference Vref internal and sample time is set to 500, to get min 12,5us sample time.
The same behafiour was seen with Vdd as reference for the Adc channel, to check if this issue is related to Vref.
To us it looks like there is and issue with the temperature sensor and it will not provide the voltage to the Adc channel.
Are there any additonal settings for the sensor or the Adc channel?
Best regards,
Jonas Maier