AM13E23019: BSEL connection

Part Number: AM13E23019

Hi,
I have following two questions related to EPI of AM13E23019.

- 1 -
I would like you to confirm how we should connect BSELx pins to memory.
According to datasheet, there is following figure.
image.png
According to TRM, it seems that "BSEL" function separate lower 8bit and higher 8bit access.

Quote from TRM ;
---
When BSEL = 1 in the EPIHB16CFG register, byte select signals are provided, so byte-sized data can be read and written at any address, however these signals reduce the available address width by 2 pins. The byte select signals are active Low. BSEL0n corresponds to the LSB of the halfword, and BSEL1n corresponds to the MSB of the halfword. 
---
However, in addition to "BSELx" pins, there is also "WRn" pin.
I'm not sure where "BSELx" pin should be connect when 16bit Host mode is used.
Could you please give connection example when BSELx pins are enabled ?

- 2 -
According to datasheet, "Data" will be valid after asserting "WRn"
image.png
Is it possible to output "Data" before asserting "WRn" pin ?

Best Regards,