Part Number: AM2612
Hello There
I am facing ADC accuracy related issue. I have configured 500 Cycles for Sampling time and and clock divisor as 8.5. I am using 12 Bit mode with internal 1.8V reference. Following is the measurements for ADC
| Input Voltage to ADC Pin | Measured ADC Counts | Voltage | Error (%) |
| 0.001 | 7 | 0.005 | |
| 0.272 | 356 | 0.2781 | 2.24 |
| 0.544 | 710 | 0.5548 | 1.99 |
| 0.816 | 1065 | 0.8322 | 1.99 |
| 1.088 | 1419 | 1.1088 | 1.91 |
| 1.359 | 1772 | 1.3847 | 1.89 |
| 1.631 | 2129 | 1.6636 | 2.00 |
| 1.903 | 2483 | 1.9403 | 1.96 |
| 2.176 | 2838 | 2.2177 | 1.92 |
| 2.445 | 3187 | 2.4904 | 1.86 |
| 2.717 | 3543 | 2.7686 | 1.90 |
| 2.988 | 3897 | 3.045 | 1.91 |
| 3.261 | 4095 | 3.2 |
Here is the plot of above information
I have a few questions
- I suspect that the internal reference is not 1.8V and because of that i am seeing this constant error of around 2%. Is there a way to measure this at the device booting ? We do not want to add external calibration mechanism.
What will be the stability of this reference voltage if we are using external calibratiion ? - If I use internal DAC calibration then upto what extent it can help us measure/calibrate the internal offsets/gain error.