AM3359: Sitara AM3359 Clock Speed Limitation

Part Number: AM3359

From the datasheet, I understand that the acceptable supported memory speeds for the EMIF memory controller is listed as a 266 MHz clock (532 MT/s data rate) for DDR2. I am also seeing that the minimum required switching characteristics for the DDR2 memory interface as per the datasheet is 3.75ns.

I am currently implementing the Alliance Memory AS4C256M8D2A-25BCN DDR2 SDRAM in my design, which has a clock frequency of 400 MHz and 800 MT/s data rate. I am trying to understand whether it is acceptable for the board to run at 400 MHz in DDR2 mode (800 MT/s data rate) and whether TI have any validation evidence proving that this is acceptable…our implementation of a 266 MHz clock (532 MT/s data rate) is causing issues with the display, but the 400 MHz clock seems to be working fine.

If a clock speed above 266 was probably not implemented at the time the datasheet was released (2016), which is why it might not have been accepted at the time?

  • 266 MHz (532 MT/s) remains the DDR2 ceiling for AM3359 as documented; the 400 MHz figures that appear in TI material refer to the DDR3/DDR PLL maximum for the AM335x family, not DDR2.

    You may need to adjust priority schemes to ensure your display receives the proper realtime data.  Please refer to the TRM section 7.3.3.5 Performance Management

    Regards,

    James