Other Parts Discussed in Thread: SYSBIOS
Hi,
I am very new to Stellaris LM4F232 controller. I have to implement Interrupt based I2C communication on LM4F232 (as a master). For that i am refering following code.
#define STATE_IDLE 0
#define STATE_WRITE_NEXT 1
#define STATE_WRITE_FINAL 2
#define STATE_WAIT_ACK 3
#define STATE_SEND_ACK 4
#define STATE_READ_ONE 5
#define STATE_READ_FIRST 6
#define STATE_READ_NEXT 7
#define STATE_READ_FINAL 8
#define STATE_READ_WAIT 9
//*****************************************************************************
//
// The variables that track the data to be transmitted or received.
//
//*****************************************************************************
static unsigned char *g_pucData = 0;
static unsigned long g_ulCount = 0;
//*****************************************************************************
//
// The current state of the interrupt handler state machine.
//
//*****************************************************************************
static volatile unsigned long g_ulState = STATE_IDLE;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
//
// The I2C interrupt handler.
//
//*****************************************************************************
void
I2CIntHandler(void)
{
//
// Clear the I2C interrupt.
//
I2CMasterIntClear(I2C0_MASTER_BASE);
//
// Determine what to do based on the current state.
//
switch(g_ulState)
{
//
// The idle state.
//
case STATE_IDLE:
{
//
// There is nothing to be done.
//
break;
}
//
// The state for the middle of a burst write.
//
case STATE_WRITE_NEXT:
{
//
// Write the next byte to the data register.
//
I2CMasterDataPut(I2C0_MASTER_BASE, *g_pucData++);
g_ulCount--;
//
// Continue the burst write.
//
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
//
// If there is one byte left, set the next state to the final write
// state.
//
if(g_ulCount == 1)
{
g_ulState = STATE_WRITE_FINAL;
}
//
// This state is done.
//
break;
}
//
// The state for the final write of a burst sequence.
//
case STATE_WRITE_FINAL:
{
//
// Write the final byte to the data register.
//
I2CMasterDataPut(I2C0_MASTER_BASE, *g_pucData++);
g_ulCount--;
//
// Finish the burst write.
//
I2CMasterControl(I2C0_MASTER_BASE,
I2C_MASTER_CMD_BURST_SEND_FINISH);
//
// The next state is to wait for the burst write to complete.
//
g_ulState = STATE_SEND_ACK;
//
// This state is done.
//
break;
}
//
// Wait for an ACK on the read after a write.
//
case STATE_WAIT_ACK:
{
//
// See if there was an error on the previously issued read.
//
if(I2CMasterErr(I2C0_MASTER_BASE) == I2C_MASTER_ERR_NONE)
{
//
// Read the byte received.
//
I2CMasterDataGet(I2C0_MASTER_BASE);
//
// There was no error, so the state machine is now idle.
//
g_ulState = STATE_IDLE;
//
// This state is done.
//
break;
}
//
// Fall through to STATE_SEND_ACK.
//
}
//
// Send a read request, looking for the ACK to indicate that the write
// is done.
//
case STATE_SEND_ACK:
{
//
// Put the I2C master into receive mode.
//
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, 0x50, true);
//
// Perform a single byte read.
//
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//
// The next state is the wait for the ack.
//
g_ulState = STATE_WAIT_ACK;
//
// This state is done.
//
break;
}
//
// The state for a single byte read.
//
case STATE_READ_ONE:
{
//
// Put the I2C master into receive mode.
//
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, 0x50, true);
//
// Perform a single byte read.
//
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//
// The next state is the wait for final read state.
//
g_ulState = STATE_READ_WAIT;
//
// This state is done.
//
break;
}
//
// The state for the start of a burst read.
//
case STATE_READ_FIRST:
{
//
// Put the I2C master into receive mode.
//
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, 0x50, true);
//
// Start the burst receive.
//
I2CMasterControl(I2C0_MASTER_BASE,
I2C_MASTER_CMD_BURST_RECEIVE_START);
//
// The next state is the middle of the burst read.
//
g_ulState = STATE_READ_NEXT;
//
// This state is done.
//
break;
}
//
// The state for the middle of a burst read.
//
case STATE_READ_NEXT:
{
//
// Read the received character.
//
*g_pucData++ = I2CMasterDataGet(I2C0_MASTER_BASE);
g_ulCount--;
//
// Continue the burst read.
//
I2CMasterControl(I2C0_MASTER_BASE,
I2C_MASTER_CMD_BURST_RECEIVE_CONT);
//
// If there are two characters left to be read, make the next
// state be the end of burst read state.
//
if(g_ulCount == 2)
{
g_ulState = STATE_READ_FINAL;
}
//
// This state is done.
//
break;
}
//
// The state for the end of a burst read.
//
case STATE_READ_FINAL:
{
//
// Read the received character.
//
*g_pucData++ = I2CMasterDataGet(I2C0_MASTER_BASE);
g_ulCount--;
//
// Finish the burst read.
//
I2CMasterControl(I2C0_MASTER_BASE,
I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
//
// The next state is the wait for final read state.
//
g_ulState = STATE_READ_WAIT;
//
// This state is done.
//
break;
}
//
// This state is for the final read of a single or burst read.
//
case STATE_READ_WAIT:
{
//
// Read the received character.
//
*g_pucData++ = I2CMasterDataGet(I2C0_MASTER_BASE);
g_ulCount--;
//
// The state machine is now idle.
//
g_ulState = STATE_IDLE;
//
// This state is done.
//
break;
}
}
}
//*****************************************************************************
//
// Write to the Atmel device.
//
//*****************************************************************************
void
AtmelWrite(unsigned char *pucData, unsigned long ulOffset,
unsigned long ulCount)
{
//
// Save the data buffer to be written.
//
g_pucData = pucData;
g_ulCount = ulCount;
//
// Set the next state of the interrupt state machine based on the number of
// bytes to write.
//
if(ulCount != 1)
{
g_ulState = STATE_WRITE_NEXT;
}
else
{
g_ulState = STATE_WRITE_FINAL;
}
//
// Set the slave address and setup for a transmit operation.
//
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, 0x50 | (ulOffset >> 8), false);
//
// Place the address to be written in the data register.
//
I2CMasterDataPut(I2C0_MASTER_BASE, ulOffset);
//
// Start the burst cycle, writing the address as the first byte.
//
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_START);
//
// Wait until the I2C interrupt state machine is idle.
//
while(g_ulState != STATE_IDLE)
{
}
}
//*****************************************************************************
//
// Read from the Atmel device.
//
//*****************************************************************************
void
AtmelRead(unsigned char *pucData, unsigned long ulOffset,
unsigned long ulCount)
{
//
// Save the data buffer to be read.
//
g_pucData = pucData;
g_ulCount = ulCount;
//
// Set the next state of the interrupt state machine based on the number of
// bytes to read.
//
if(ulCount == 1)
{
g_ulState = STATE_READ_ONE;
}
else
{
g_ulState = STATE_READ_FIRST;
}
//
// Start with a dummy write to get the address set in the EEPROM.
//
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, 0x50 | (ulOffset >> 8), false);
//
// Place the address to be written in the data register.
//
I2CMasterDataPut(I2C0_MASTER_BASE, ulOffset);
//
// Perform a single send, writing the address as the only byte.
//
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_SINGLE_SEND);
//
// Wait until the I2C interrupt state machine is idle.
//
while(g_ulState != STATE_IDLE)
{
}
}
//*****************************************************************************
//
// This example demonstrates the use of the I2C block to connect to an Atmel
// AT24C08A EEPROM.
//
//*****************************************************************************
int
main(void)
{
unsigned char pucData[16];
unsigned long ulIdx;
//
// Set the clocking to run directly from the crystal.
//
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_6MHZ);
//
// Init the PDC and the LCD.
//
PDCInit();
PDCLCDInit();
PDCLCDBacklightOn();
//
// Enable the peripherals used by this example.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Indicate that the I2C example is running.
//
PDCLCDSetPos(0, 0);
PDCLCDWrite("I2C running...", 14);
//
// Enable processor interrupts.
//
IntMasterEnable();
//
// Configure the appropriate pins to be I2C instead of GPIO.
//
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_2 | GPIO_PIN_3);
//
// Initialize the I2C master.
//
I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet(), false);
//
// Enable the I2C interrupt.
//
IntEnable(INT_I2C0);
//
// Enable the I2C master interrupt.
//
I2CMasterIntEnable(I2C0_MASTER_BASE);
//
// Write a data=address pattern into the first 16 bytes of the Atmel
// device.
//
for(ulIdx = 0; ulIdx < 16; ulIdx++)
{
pucData[ulIdx] = ulIdx;
}
AtmelWrite(pucData, 0, 16);
//
// Read back the first 16 bytes of the Atmel device and verify that it
// contains the data it should.
//
AtmelRead(pucData, 0, 16);
for(ulIdx = 0; ulIdx < 16; ulIdx++)
{
if(pucData[ulIdx] != ulIdx)
{
PDCLCDSetPos(0, 1);
PDCLCDWrite("Data error.", 11);
while(1)
{
}
}
}
//
// Success.
//
PDCLCDSetPos(0, 1);
PDCLCDWrite("Success.", 8);
//
// Finished.
//
while(1)
{
}
}
I have some Questions in this code
1. Why "STATE_WAIT_ACK and STATE_SEND_ACK" states are used.(We dont do these steps while polling based transmission). Actually we finish sending of data after sending I2C_MASTER_CMD_BURST_SEND_FINISH.
2. As we will get interrupt after sending each byte. is it neccesory to check transmission error at start of ISR Routine. why in this code error is check at state STATE_WAIT_ACK? i.e after compliting whole transaction(after getting STOP bit) .