Other Parts Discussed in Thread: TMS570LS3137
Hello,
I'm working on a project that utilizes the FlexRay controller and the information about where the FlexRay pins are located seems to
conflict in different cources. The datasheet to TMS570LS3137 (http://www.ti.com/lit/ds/spns162/spns162.pdf) shows that the pin numbers
are 1; 2; 5; 126; 133 and 142. It also says that the pin layout picture depicts only the default function. So I would assume that FR
is the default function, since it's in the picture.
But if I look into the User's guide (http://www.ti.com/lit/ug/spnu499/spnu499.pdf) and go to the IOMM part there it says that default
functions of pins 1 and 2 are GIOB[3] and GIOA[0]. Ass a matter of fact I can't find FR anywhere in the IOMM PINMMRnn table.
So which pins belong to the FlexRay and how do I enable them?
Thanks for any advice