Hello, TI.
I used to RM48 HDK.
I measured the voltage using ADC Module results are summarized as follows.
Voltage Conversion Result
0V -> 0
1V -> about 790
2V -> about 1610
3V -> about 2389
4V -> about 3123
5V -> 4095
condition: VREFHI : 5V, VREFLO : 0V
So, I read the TRM.
Can i get the Calibration Error & Mid-Point Calibration Example Code ?
Thank you, I wait for TI's Reply.